KAS Simulator Menus Description

File Menu

Command

Description

Start

Start the application with the Retain Variables.

Cold Start

Start the application with the initial settings.

Stop

Stop the application.

Option

Set parameters for the KAS Simulator application (see explanations below).

Exit

Leave KAS Simulator application.

Option

Options for Simulator

Option

Description

Autostart

Autostart the application when KAS Simulator is launched.

Autostart mode is recommended when a system is in production.


  • Parameters are saved in the Options.bin file located under:
    <user>\AppData\Local\Kollmorgen\KAS\Sinope Simulator\Resources\

Help Menu

Command

Description

About

Show version numbers and other Find the KAS-IDE Version about KAS Simulator